25.2.1 BiSS Frame
In the following point-to-point configuration, a simple example of a BiSS frame is shown. Figure 25-5 shows the clock generated on MA and transmitted to the client. In this case, the client is a sensor, and a packet of data is sent from the sensor or client back to the host.
Note: See Bus Protocol Details for more
information regarding the BiSS frame label definitions.