2.118.4 TRAM_RAMGet Function
C
bool TRAM_RAMGet( uint32_t ramIndex, uint32_t *data );
Summary
Reads data from the TrustRAM RAMx register
Description
This function is used to read 32-Bit data from the TrustRAM RAM[ramIndex] register.
Precondition
None
Parameters
Param | Description |
---|---|
ramIndex | Specifies the index of the RAM register to be written to |
*data | Pointer to the user buffer to store the data read from RAM[index] register |
Returns
true - If data is read successfully
false - If the ramIndex is out of range
Example
uint32_t data; // Read Data from TrustRAM's RAM0 register TRAM_RAMGet(0, &data);
Remarks
None.