2.113.1.33 TCx_Compare32bitCounterSet Function
C
/* x = TC instance number */
void TCx_Compare32bitCounterSet( uint32_t count );
Summary
Sets new timer counter value.
Description
This function sets new timer counter value.
Precondition
TCx_CompareInitialize() function must have been called first.
Parameters
Param | Description |
---|---|
count | new counter value to set |
Returns
None.
Example
uint32_t count = 0x100;
TC0_CompareInitialize();
TC0_CompareStart();
TC0_Compare32bitCounterSet(count);
Remarkss
The caller must know the number of significant bytes of timer. Counter value is right-aligned.