2.42.5 EVSYS_UserDisable Function
C
void EVSYS_UserDisable(void)
Summary
Disables EVSYS user
Description
This function disables the EVSYS User.
Precondition
EVSYS module should be initialized with the required configuration parameters from the MCC GUI in the EVSYS_Initialize() function
Parameters
None
Returns
None
Example
// Disable Event System user
EVSYS_UserDisable();
Remarks
The EVSYS_UserDisable API should be used to disable user at run time.