2.24.3 DACC_ChannelDataWrite Function
C
void DACC_ChannelDataWrite(DACC_CHANNEL_NUM channel, uint16_t data)
Summary
Converts a Digital data to Analog value
Description
This function converts a Digital data to Analog value. The behavior of this function call will vary based on the mode selected within MCC.
Precondition
DACC_Initialize must have been called.
Parameters
Param | Description |
---|---|
channel | Points to DACC Channel |
data | Digital data to be converted to Analog value. |
Returns
None
Example
char myData[COUNT] = {"0xff","0x3E","0x7A","0x3F"};//COUNT is user dependent for (uint8_t i = 0; i<4; i++) { DACC_ChannelDataWrite (DACC_CHANNEL_0, myData[i]); }
Remarks
This API should be used when TAG is enabled.