2.24.5 DACC_DataWrite Function

C

The prototype of this function varies based on device family. Refer to the generated header file for the actual prototype to be used.

void DACC_DataWrite (DACC_CHANNEL_NUM channel, uint32_t data)
void DACC_DataWrite(uint16_t data)

Summary

Converts a Digital data to Analog value

Description

This function converts a Digital data to Analog value. The behavior of this function call will vary based on the mode selected within MCC.

Precondition

DACC_Initialize must have been called.

Parameters

ParamDescription
channelPoints to DACC Channel
dataDigital data to be converted to Analog value.

Returns

None

Example

Example of this function varies based on device family. Refer to the one which is applicable for the device being used.

char myData[COUNT] = {"0xff","0x3E","0x7A","0x3F"};//COUNT is user
    //dependent
    bool status = false;
    
    //considering count = 4
    for (uint8_t i = 0; i<4; i++)
    {
        DACC_DataWrite (DACC_CHANNEL_0, myData[i]);
    }
bool status = false;
DACC_ChannelSelect(DACC_CHANNEL_0);
if (true == DACC_IsReady())
{
    DACC_DataWrite (0xff);
}
else
{
    //DACC is not ready to accept new conversion request
    //User Application code
}

Remarks

None.