2.121.7 TWIx_TransferSetup Function
C
/* x = TWI instance number */
/* TWI master mode */
bool TWIx_TransferSetup(TWI_TRANSFER_SETUP* setup, uint32_t srcClkFreq)
Summary
Dynamic setup of TWI Peripheral.
Description
This API is generally used when there are multiple clients on the same TWI bus having different clock speed. In such a case, the TWIx_TransferSetup API must be called to set the appropriate bus speed before starting the TWI transfer for the TWI slave.
Precondition
TWIx_Initialize must have been called for the associated TWI instance. The transfer status should not be busy.
Parameters
Param | Description |
---|---|
setup | Pointer to the structure containing the transfer setup. |
srcClkFreq | TWI Peripheral Clock Source Frequency. |
Returns
true - Transfer setup was updated Successfully.
false - Failure while updating transfer setup.
Example
TWI_TRANSFER_SETUP setup; setup.clkSpeed = 400000; // Make sure that the TWI is not busy before changing the TWI clock frequency if (TWI1_IsBusy() == false) { if (TWI1_TransferSetup( &setup, 0 ) == true) { // Transfer Setup updated successfully } }
Remarks
srcClkFreq overrides any change in the peripheral clock frequency. If configured to zero PLIB takes the peripheral clock frequency from MCC.