2.121.6 TWIx_ErrorGet Function
C
/* x = TWI instance number */
/* TWI master mode */
TWI_ERROR TWIx_ErrorGet(void)
Summary
Returns the TWI error that occurred on the bus.
Description
This function returns the TWI error that occurred on the bus. The function can be called to identify the error cause.
Precondition
TWIx_Initialize must have been called for the associated TWI instance.
Parameters
None.
Returns
Returns error of type TWI_ERROR, identifying the error that has occurred.
Example
if(TWI1_ErrorGet() == TWI_ERROR_NONE) { //Transfer is completed successfully } else { //Error occurred during transfer. }
Remarks
None