2.119.2 TRNG_RandomNumberGenerate Function
C
void TRNG_RandomNumberGenerate( void )
Summary
Initiates generation of random number using the TRNG peripheral in interrupt mode.
Description
This function triggers the TRNG peripheral to generate a 32-bit random number in interrupt mode.
The generated random number will be passed to the registered callback function once ready.
Precondition
None.
Parameters
None.
Returns
None.
Example
uint32_t random_number;
void testCallback( uint32_t random, uintptr_t context)
{
random_number = random;
}
TRNG_CallbackRegister(testCallback, NULL);
TRNG_RandomNumberGenerate();
Remarks
This API is only generated when the interrupt mode is enabled.