2.113.2.3 TCx_CHy_TimerPeriodHasExpired Function
C
/* x = TC instance number, y= channel number */ bool TCx_CHy_TimerPeriodHasExpired ( void );
Summary
Checks whether timer period is elapsed
Description
This function checks the status of the timer period interrupt.
Precondition
TCx_CHy_TimerInitialize() function must have been called first for the given channel.
Parameters
None
Returns
-
True - timer period has expired
-
False - timer period is not expired
Example
bool status; TC0_CH1_TimerInitialize(); status = TC0_CH1_TimerPeriodHasExpired();
Remarks
This function is available only in polling mode