2.98.6 SDADC_ConversionResultGet Function
C
int16_t SDADC_ConversionResultGet( void )
Summary
Returns the conversion result.
Description
This function returns the result of completed conversion.
Precondition
SDADC_Initialize() function must have been called first for the associated instance.And conversion must have been started.
Parameters
None.
Returns
Returns 16 bit signed conversion result.
Example
int16_t sdadcResult = 0;
SDADC_Initialize();
SDADC_ConversionStart();
sdadcResult = SDADC_ConversionResultGet();
Remarks
This function can be called from interrupt or by polling the status when result is available.