9.15.9.12 Example
Opens the 'FPPrj1.pro' project from the FPProject1 directory
open_project -project {./FPProject1/FPPrj1.pro}
paste_device
Pastes the devices that are on the clipboard in the chain, immediately above the position_name device, if this parameter is specified. Otherwise it places the devices at the end of the chain. The chain programming mode must be enabled.
paste_device [-position_name {position_name}]