9.15.9.21 Arguments
-name {device_name}
Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command.
-file {filename}
(Optional) Identifies the name of the file to which read results will be saved.