9.15.9.33 Arguments

-name device_name

Optional user-defined device name. The device name is not required if there is only one device in the current configuration, or a device has already been selected using the set_debug_device command.

-mapping {logical | physical}

(Optional) Specifies how the data read from the UFROM is mapped. Values are explained in the table below.

Value

Description

logical

Logical mapping (default)

physical

Physical mapping

-file {filename}

(Optional) Identifies the name of the file to which read results will be saved.