5.22.12 Default Tie-offs with Bus Interfaces
Bus definitions can contain default values for each of the defined signals. These default values specify what the signal should be tied to if it is mapped to an unconnected input pin on the instance.
Bus definitions are specified as required connection vs optional connection that defines the behavior of tie-offs during SmartDesign generation.
Required bus interfaces - The signals that are not required to be mapped will be tied off if they are mapped to an unconnected input pin.
Optional bus interfaces - All signals will be tied off if they are mapped to an unconnected input pin.