5.22.7 Modifying Bus Interface Details
Only bus interfaces that you explicitly added to an instance can be modified. Bus interfaces that were instantiated as part of core generation cannot be modified.
To modify the properties of a bus interface:
- In the Canvas, select the bus interface pin object, right-click, and
choose Modify Bus Interface .
Figure 5-60. Modify Bus Interface Dialog Box
- Modify the bus interface details, configuration parameters, or signal map definition and click OK.
Map By Name attempts to map any similar signal names between the bus definition and pin names on the instance.