19.10 Unassigning pins
Unassign an I/O macro from a locked assignment when its locked position is no longer required. Unassigned macros are automatically placed in optimum locations during layout.
To unassign a macro from a pin:
- Select the I/O macro in the Assigned list box.
- Unassign the selected macro from
a pin location using any one of these methods:
- Drag the selected macro name from the Assigned list box to the Unassigned list box.
- From the Edit menu, choose Unassign.
- Click the Unassign toolbar button.
- Press the DELETE key.
- In the I/O Attribute Editor, select Unassign in the Pin # cell. The macro is unassigned.