5.6.4.1 DO file

Use automatic DO file - Select if you want the Project Manager to automatically create a DO file that will enable you to simulate your design.

User defined DO file - Enter the DO file name or click the browse button to navigate to it.

Simulation Run Time - Specify how long the simulation should run. If the value is 0, or if the field is empty, there will not be a run command included in the run.do file.

Testbench module/entity name - Specify the name of your testbench entity name. Default is “testbench,” the value used by WaveFormer Pro.

Top Level instance name in the testbench - Default is <top_0>, the value used by WaveFormer Pro. The Project Manager replaces <top> with the actual top level macro when you run ModelSim.

DO command parameters - Text in this field is added to the DO command.

Generate VCD file - Click the checkbox to generate a VCD file.

VCD file name - Specifies the name of your generated VCD file. The default is power.vcd; click power.vcd and type to change the name.