13.31.3.1 Generate a Programming File

To generate a programming file:
  1. Select the Silicon feature(s) you want to program.

    FPGA Array

    FlashROM

  2. Click Next or Finished depending on the silicon features you selected.

If you click Next, follow the instructions in the appropriate dialog box. If you click Finish, the Generate Programming Files dialog box appears. Use this dialog box box to specify the programming file name, location, and output format (STAPL file, SVF file, PDB file, DirectC DAT file, 1532 file).

For more information on DAT files, refer to the Data File Generator (DatGen) section of the DirectC User's Guide.