5.32.13 Custom Serialization Data for FlashROM Region

FlashPoint enables you to specify a custom serialization file as a source to provide content for programming into a Read from file FlashROM region. You can use this feature for serializing the target device with a custom serialization scheme.

To specify a FlashROM region:

  1. From the Properties section in the FlashROM Settings page, select the file name of the custom serialization file (see the figure below). For more information on custom serialization files, see Custom Serialization Data File Format.
Figure 5-126. FlashROM Settings
???
  1. Select the FlashROM programming file type you want to generate from the two options below:
    • Single programming file for all devices option: generates one programming file with all the values in the custom serialization file.
    • One programming file per device: generates one programming file for each value in the custom serialization file.
  2. Enter the number of devices you want to program.
  3. Click the Target Programmer button.
  4. Select your target Programmer type.
  5. Click OK.