13.23.18 Synthesizing Your Design with Synplify
- In the Libero IDE, right-click the HDL file in the Files tab, or the top-level schematic for mixed schematic-HDL designs in the Hierarchy, and select Synthesize. Synplify starts and loads the appropriate design files, with a few pre-set default values.
- From Synplify’s Project menu, choose Implementation Options.
- Set your specifications and click OK.
- Deactivate synthesis of the defparam
statement. The defparam statement is only for simulation tools and is not intended for
synthesis. Embed the defparam statement in between translate_on and translate_off
synthesis directives as follows :
/* synthesis translate_off */
defparam M0.MEMORYFILE = "meminit.dat"
/*synthesis translate_on */
// rest of the code for synthesis
- Click the RUN button. Synplify
compiles and synthesizes the design into an EDIF, *.edn, file. Your EDIF netlist is then
automatically translated by Libero into an HDL netlist. The resulting *edn and *.vhd files
are visible in the File Manager, under Implementation Files.
Should any errors appear after you click the Run button, you can edit the file using the Synplify editor. Double-click the file name in the Synplify window showing the loaded design files. Any changes you make are saved to your original design file in Libero.
- From the File menu, choose Exit to close Synplify. A dialog box asks you if you would like to save any settings that you have made while in Synplify. Click Yes.
Note:
- See the Microchip Attribute and Directive Summary in the Synplify online help for a list of attributes related to Microchip devices.
- To add a clock constraint in Synplify you must add "n:<net_name>" in your SDC file. If you put the net_name only, it does not work.