5.32.14.2 Hex serialization data file example
The following example is a Hex serialization data file for a 40-bit region. Enter the serialization data below into file created by any text editor:
123AEd210 AeB1 0001242E
If you enter an invalid Hex digit such as 235SedF1, an error occurs. An error will also occur if you enter data that is out of range, i.e. 4300124EFE.
The following is an example of programming "AeB1" into Region_7_1 located on page 7, from Word 5 to Word 1 in the FlashROM settings page. See Custom serialization data for FlashROM region for more information.
Table 15 | ... | Word 5 | Word 4 | Word 3 | Word 2 | Word 1 | Word 0 | ||
Page 7 | ... | ... | ... | 00 | 00 | 00 | AE | B1 | ... |