7.4 Creating Pins and Ports for Connecting Instances in the SmartDesign
(Ask a Question)After placing the components in your SmartDesign canvas, you now need to create pins and ports to connect the various instances to complete your design.
Each pin or port has a direction and a type. Direction of the regular ports (non-Bus Interface ports) can be input, output, and bidirectional (inout).
The following is a list of types of pins or ports:
- Scalar: Single unit-level signal
- Bus: Array of scalar
ports. The range of the bus ports are indicated by square brackets
[nFirst:nLast]
. For Example,busName[3:0]
. - Slice: Slice is a part of
a bus port. A bus slice is of any range size within the bus range. For example,
sliceName[0]
,sliceName[2:0]
. - Bus Interface (BIF): A Bus
Interface is a bundle of scalar or bus ports that has functional meaning to it. BIF ports
have characteristics such as functional types and roles that define how two Bus Interfaces
can connect to one another. SmartDesign provides a rich set of AMBA Bus
Interfaces–
AXI
,AXI4
,AXI4Stream
,AHB
,AHBLite
, andAPB3
– to help create easily AMBA sub-systems. It also provides Microchip specific Bus Interface types for easy connectivity between Microchip hardware components.
Scalar ports or pins in SmartDesign may have a PAD characteristic property. A pin or port with a PAD property must be connected to a top-level port of the design. PAD ports eventually assign to a package pin. In SmartDesign, these ports are automatically promoted to the top-level and can be modified, if needed.
For better organization of the instance pins, you can create groups. Groups are displayed on an instance with a Group pin that is just a visual representation and cannot be connected. Any pin can be added or removed from the group. Groups can be collapsed to hide member pins.
7.4.1 Creating Pins and Ports for your Design
(Ask a Question)After placing the components in your SmartDesign canvas, you now need to create pins and ports to connect the various instances to complete your design.
Each pin or port has a direction and a type. Direction of the regular ports (non-Bus Interface ports) can be input, output, and bidirectional (inout).
- You can create a pin or port in either of the
following ways:
- On the menu, click
- On the SmartDesign toolbar, click Add Port
Result: The Add Port dialog appears.
- Enter an appropriate and unique name for the port
in the Name box. You can specify a bus port by indicating the bus
range directly into the name using brackets [ ]. For example, mybus[3:0]. Important: If the port name violates HDL naming rules, an error message is printed in the Log window, and the new port is not created.
- Choose the pin or port type that you want to
create as per the following table and then click OK. The chosen port
type is created in the SmartDesign canvas.
Pin or Port Type Representation Purpose Input Input port for operating with inputs. By default, the input pins and ports are placed on the left side of the canvas. Output - Unconnected - Connected Output port for operating with outputs. By default, the output pins and ports are placed on the right side of the canvas.
Bi-directional (inout) - Unconnected - Connected Bi-directional port for operating as an input or an output pin or port. By default, the bi-directional pins and ports are placed on the right side of the canvas.
7.4.2 Modifying the Pin Order
(Ask a Question)If the outputs of one component (instance A) communicate with the inputs of another component (instance B) and otherwise, nets may intersect with each other and the view may be cluttered. To prevent this, the Modify Pin Order functionality allows you to modify the default pin placement of the instance.
To modify the default pin placement of the instance:
-
Right-click the component and select Modify Pin Order Help dialog box appears.
from the right-click menu. The - Follow the instructions in Modify Pin Order Help dialog box to move
the pin.A pin that has been moved away from default locations is identified by a bold arrowhead. An inward-pointing arrowhead indicates an input pin and an outward-pointing arrowhead indicates an output pin. Inout pins do not have an arrowhead when they are moved away from the default locations (right side of instance).
- To reset the instance pin order to its default order, right-click the instance, and select from the right-click menu.
7.4.3 Performing Operations on Pins or Ports
(Ask a Question)When one or more pins or ports are selected, you can use the right-click menu to perform the following operations on the ports and pins.
Operation | Action |
---|---|
Connect | The Connect command connects the selected pins and ports with a net. If there is a net selected, it is used to make the connection. This is the only pin or port action that takes selected nets into account. If the connection is not possible, an error message is printed in the Log window. A connection is established only if all the selected objects can be connected. |
Disconnect | The Disconnect command disconnects all the selected non-pad pins or ports from their attached net. |
Promote to Top-Level | The Promote to Top-Level command is available to all
non-PAD pins. It creates a port and a net connecting the port to the pins or slices.
If a port with the same name already exists, a new unique port name is created. For
example, if a BIF ( |
Go to Driver | The Go to Driver command zooms onto the driver of the selected pin or port. The Go to Driver command is not available for output pins and input ports. The driver cannot be an inout. |
Magnify Pin | Double-click a pin/port or right-click and select Magnify
Pin to zoom into the pin/port connection. The Magnify
Pin window shows the specified pin/port connections. If the pin has a fanout of more than one, the number beside the + sign on the right shows the total fanout count. Click the + sign to see all the fanouts of the pin. You can double-click the net, pin, port, or instance inside the Magnify window to zoom and select the item. |
Modify/Rename | The Modify or Rename command opens
a Modify Port dialog box. You can change the port name and the
range of the port. Note:
|
Delete | The Delete command deletes all the selected items that can
be deleted: slices, user created groups, group members, and ports. The Delete command deletes all the selected items, even if the selected items are of different types. When a group member is deleted, the member is deleted from the group only. The actual pin is not deleted. |
Mark Unused | This option is available to the output pins (scalar, bus, and BIF) of an instance. The Mark Unused command allows you to show the output pins that are not being used in the design and must not be flagged as a warning when generating the design or running the DRC operation. |
Invert | The Invert command inverts the input or output scalar pin and port. A bubble is added to indicate inversion. |
Tie High | The Tie High command connects the pin (scalar and bus) to a logical 1. For a bus pin, this action deletes all slices. For a group, this action is applied to all non-output member pins in the group. |
Tie Low | The Tie Low command connects the pin (scalar and bus) to a logical 0. For a bus pin, this action deletes all slices. For a group, this action is applied to all non-output member pins in the group. |
Tie Constant | The Tie Constant command is available only to bus pins and slices (except single-bit slice). It opens the Tie to Constant dialog box for a constant value in HEX to be entered for the bus pins and slices. |
Clear Attributes | The Clear Attributes command clears the pin attributes (Tie to High, Low, Constant, Inversion, or Marked Unused). |
Highlight | The Highlight option opens a menu with multiple highlight
color selections. Select a color to highlight the selected items. If any items are
already highlighted, then choosing a different color highlight changes from the
previous highlight color. This option is available when a single or multiple
instances, nets, and ports are selected. If you highlight an instance, it automatically highlights the non-highlighted pins of the instance. Click the Unhighlight all icon ( ) in the toolbar to remove the highlight color of all highlighted design objects, including highlighted nets. The Highlight option is also available in the right-click menu of the low-level instances in the Expanded Inplace view. |
Bus and Slice operations | When a bus, slice pins, or ports are selected, the right-click menu in addition to regular pin actions have additional commands. For more information, see 7.4.4 Working with Bus and Slice. |
Add Pin to New Group and Add Pin to Group | This menu item is available to instance pins. When a group is selected,
right-click a pin and choose Add Pin to Group to add the pin to
the selected group. If no group is selected, the Add Pin to New
Group command is available and creates a new group with the default
group name, such as Group, Group_1,
Group_2, Group_3, and all the selected
pins are added to the newly created group. A pin group is expanded to display the member pins or is collapsed to hide the member pins. If a group is collapsed, pins that are not connected to nets or have attributes (tied low or high, tied to constant, and marked unused) are hidden. |
Rename (Group) | Group pins, unlike other instance pins, can also be renamed. Right-click
Group and choose Rename. The
Rename Group dialog box appears. You can choose to change the
name of the group in this dialog box and click OK to apply the
changes. If an invalid name is entered or a pin with that name already exists, then an error message is printed in the Log window. |
7.4.4 Working with Bus and Slice
(Ask a Question)You can perform the following operations on a Bus or Slice using the right-click menu options:
- Flip Bit
Order: This command is available only for slices. This option allows you
to flip the slice range. For example,
mySlice[10:0]
is flipped tomySlice[0:10]
of the slice. All connection or tieoff information and presentation information is retained. - Create Slice:
This command opens a menu of slice options that can be created from the bus pin or
ports. The custom slice(s) option can be used to create any slice or bit combination
of your choice. For example, using a 32-bit bus with the Custom Slices option allows
you to create any slice or bit combinations (For example, a slice of 10 bits and
another slice of 22 bits). To make it convenient to create slices, common slice
ranges for the selected bus are listed in the list. For example,
- 32 slices of width 1
- 16 slices of width 2
- 8 slices of width 4
- 4 slices of width 8
- 2 slices of width 16
The directions of the slices (input or output) are indicated by an arrowhead and match the bus pin or port direction. On a bus port, the slices are placed in a column behind the bus port.
Important: If slices existed before, the predefined slices are created and the existing slices are deleted before creating the new ones. - Custom Slices:
This command opens the Add Slice(s) dialog box for entering a
list of slices. If these slices are all valid, they are added to the bus. If the slices are
not valid (For example, out-of-range slices, overlapping slices for input pins
(output ports), or existing slices), the error is printed in the
Log window. The dialog box supports any separator
character except colon because the colon is used to specify a range. No characters
other than the colon are allowed to be adjacent to the two-range indices.Tip: Creating a Custom Slice does not delete any pre-existing slices.
- Edit Slice:
This command opens the Edit Slices dialog box. You can choose
to delete, modify, and create a new slice, if required.Use the dialog box to change the range of the bits, add a slice, or delete a slice. If you specify invalid range values, an error icon appears in the Edit Slices dialog box. Hover your cursor over the error icon to display the error message.
- Pins to
Expose: This command opens the Pins to Expose
dialog box displaying all the Bus Interface pins that can be
exposed or hidden.
In the dialog box, you can check the pins in the BIF that you want to expose and deselect the ones that you want to be hidden. Hidden BIF pins are not visible in the SmartDesign canvas.
Important: Not all pins can be exposed. If a BIF pin is already connected, none of the input pins can be exposed. If a BIF pin is not connected, every item in the menu can be exposed.