3.5.1.24.2 SoC Data Transfer Methods
(Ask a Question)There are three data transfer methods provided to transfer data between processor memory and HLS accelerators.
- CPU Copy
The RISC-V CPU handles the data transfer between memory and the accelerator’s on-chip memory buffer. This transfer method is available for pointer arguments specified with the AXI4 Target Interface for Pointer Argument (e.g.,
#pragma HLS interface argument(<ARGUMENT_NAME>) type(axi_target)
). Thememcpy_write
andmemcpy_read
driver functions are used to initiate the CPU Copy transfers in and out of the accelerator’s on-chip memory buffer (see Pointer Argument Driver Functions). The CPU copy method is used when thedma
option of the AXI4 target interface pragma is unspecified or is set to false, where the Top-level Driver Functions call thememcpy_write
function for the RISC-V CPU to transfer argument data from processor memory to the accelerator’s on-chip memory buffer before the accelerator starts executing (if data is used as an input to the accelerator), and call thememcpy_read
function for the RISC-V CPU to copy data from the accelerator’s on-chip memory buffer back to processor memory after accelerator finishes execution (if data is used as an output from the accelerator). If data is used as both input and output, bothmemcpy_read
andmemcpy_write
are called (see Top-level Driver Options in Pointer Arguments' AXI4 Target Interface Pragma).- DMA Copy
A DMA core transfers data between processor memory and accelerator’s on-chip memory buffer in bursts to achieve high bandwidth data transfer. As in the CPU Copy method, this transfer method is available for pointer arguments specified with the AXI4 Target Interface for Pointer Argument and is used when the
dma
option is set to true (e.g.,#pragma HLS interface argument(<ARGUMENT_NAME>) type(axi_target) dma(true)
). Thedma_write
anddma_read
driver functions are used to initiate DMA Copy transfers in and out of the accelerator’s on-chip memory buffer (see Pointer Argument Driver Functions). When the DMA Copy method is used, the Top-level Driver Functions call thedma_write
anddma_read
functions to copy data in and out of the accelerator’s on-chip memory buffer depending on the argument’s direction (also see Top-level Driver Options in Pointer Arguments' AXI4 Target Interface Pragma).Important:For pointer arguments specified with AXI4 target interface pragma, both CPU and DMA Copy transfer methods can be used. The generated accelerator architecture is the same for both transfer methods, with the difference being the driver functions that are used to perform the data transfers. Users can call the appropriate driver functions or simply change the
dma
option in the interface pragma to configure the transfer method used by the Top-level Driver Functions and no hardware recompilation would be required.- Accelerator Direct Access
This method can only be used when an AXI4 Initiator interface is specified for a pointer argument with the
#pragma HLS interface argument(<ARGUMENT_NAME>) type(axi_initiator)
pragma (see AXI4 Initiator Interface for Pointer Argument ). In this case, the accelerator will directly access the processor memory This method has the advantage that no on-chip memory buffer is required in the accelerator as it accesses data directly without it being copied, resulting in lower on-chip memory usage. This method is recommended when data is not accessed frequently, as the latency for the accelerator to access processor memory will be higher than accessing accelerator’s on-chip memory buffer, and is not recommended when large amounts of data needs to be accessed.As described above, the accelerator’s architecture will be different depending on which data transfer method is being used. Using CPU Copy and DMA Copy will result in on-chip memory buffer being created for AXI Target interface to store the copied data, and using Accelerator Direct Access will not create on-chip memory buffer for AXI Initiator interface.