21.9.22 smartpower_init_set_othersets_options
(Ask a Question)Description
This Tcl command initializes the frequency and probability of all other sets.
Note: This command is associated with the functionality of Initialize Frequencies and Probabilities dialog box.
smartpower_init_set_othersets_options \
[-freq "decimal value [unit { Hz | KHz | MHz }]"] \
[-proba "decimal value"] \
[-with "fixed | default"] \
[-input_freq "decimal value [unit { Hz | KHz | MHz }]"] \
[-input_proba "decimal value"]
Arguments
Parameter | Type | Description |
---|---|---|
freq | string | Specifies the default frequency and units(possible values are Hz, KHz or MHz). This parameter is optional. |
proba | decimal | Specifies the default probability. Must be positive decimal value, less than or equal to 100.000. This parameter is optional. |
with | string | Specifies vectorless or default analysis. This parameter is optional. |
input_freq | decimal | Specifies the input frequency(decimal possible value) and units(possible values are Hz, KHz or MHz). This parameter is optional. |
input_proba | decimal | Specifies the input probability. Must be positive decimal value, less than or equal to 100.000. This parameter is optional. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | input_proba: Invalid argument value: 'value' (expecting decimal value). |
None | Parameter 'input_proba' has illegal value. |
None | Parameter 'input_proba' must be less than or equal to 100.000. |
None | Parameter 'input_proba' must be a positive decimal value. |
None | input_freq: Parameter format incorrect (expecting a positive decimal value, optionally followed by a unit (possible values are Hz, KHz or MHz)). |
None | Parameter 'input_freq' has illegal value. |
None | with: Invalid argument value: 'value' (expecting default or fixed). |
None | Parameter 'with' has illegal value. |
None | proba: Invalid argument value: 'value' (expecting decimal value). |
None | Parameter 'proba' must be less than or equal to 100.000. |
None | Parameter 'proba' must be a positive decimal value. |
None | Parameter 'proba' has illegal value. |
None | freq: Parameter format incorrect (expecting a positive decimal value, optionally followed by a unit (possible values are Hz, KHz or MHz)). |
None | Parameter 'freq' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_init_set_othersets_options [-freq "decimal value [ unit { Hz | KHz | MHz } ]"] [-proba "decimal value"] [-input_freq "decimal value [ unit { Hz | KHz | MHz } ]"] [-input_proba "decimal value"]'. |
Supported Families
PolarFire® |
SmartFusion® 2 |
RTG4™ |
IGLOO® 2 |
PolarFire SoC |
Example
The following example initializes all other sets after executing "smartpower_init_do" with "-othersets {true}":
Note: Warning: -with flag is obsolete; use -with argument of the command smartpower_init_do instead.
smartpower_init_set_othersets_options \
-freq "10 MHz" \
-proba "10" \
[-with "fixed"] \
-input_freq "10 MHz" \
-input_proba "10"