21.9.25 smartpower_init_set_set_reset_options
(Ask a Question)Description
This Tcl command initializes the frequency and probability of all set and reset nets.
smartpower_init_set_set_reset_options \
[-freq "decimal value [unit { Hz | KHz | MHz | % }]"] \
[-proba "decimal value"]
Arguments
Parameter | Type | Description |
---|---|---|
freq | decimal | Specifies the user input frequency (in Hz, KHz, or MHz) or the toggle rate (in %). If the unit is not provided and toggle rate is active, the value is handled as a toggle rate, if toggle rate is not active, the value is handled as a frequency. This parameter is optional. |
proba | decimal | Specifies the user input probability in persentage(%). This parameter is optional. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'proba' must be a positive decimal value. |
None | Parameter 'proba' must be less than or equal to 100.000. |
None | proba: Invalid argument value: 'value' (expecting decimal value). |
None | proba: Invalid argument value: 'value' (expecting decimal value). |
None | Parameter 'proba' has illegal value. |
None | freq: Parameter format incorrect (expecting a positive decimal value, optionally followed by a unit (possible values are Hz, KHz, MHz or %)). |
None | Parameter 'freq' has illegal value. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_init_set_set_reset_options [-freq "decimal value [unit { Hz | KHz | MHz | % }]"] [-proba "decimal value"]'. |
Supported Families
PolarFire® |
SmartFusion® 2 |
RTG4™ |
IGLOO® 2 |
PolarFire SoC |
Example
The following example initializes all set/reset nets after executing "smartpower_init_do" with "-set_reset {true}":
smartpower_init_do -set_reset {true}
smartpower_init_set_set_reset_options -freq {10 MHz} -proba {20}