21.9.12 smartpower_export_mpe_report
(Ask a Question)Description
This Tcl command exports the Microchip Power Estimation(MPE) report in XML format. The generated
.xml
report contains the following information: - Device Settings
- Thermal Settings
- Voltage Source
- Clocks
- Logic Breakdown
- LSRAM Breakdown with Advanced Settings
- uSRAM Breakdown with Advanced Settings
- Math Breakdown with Advanced Settings
- PLL and DLL
- I/Os
- Crypto
- Transceivers
In addition, the following information is available for PolarFire SoC devices:
- MSS RISC-V (Quad U54)
- AXI MSS/Fabric Interfaces
- MDDR
- MSS I/O Interfaces
- User Crypto
Note: This command supported only for G5 families.
smartpower_export_mpe_report -filename {file_name.xml}
Arguments
Parameter | Type | Description |
---|---|---|
file_name | string | Name of the XML file to be exported. This argument is mandatory. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'filename' has illegal value. |
None | Required parameter 'filename' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_export_mpe_report -filename "filename"'. |
Supported Families
PolarFire® |
PolarFire SoC |
Example
The following command exports the Microchip Power Estimation (MPE) report in mpe_report.xml file:
smartpower_export_mpe_report -filename {mpe_report.xml}