21.9.54 smartpower_set_voltage_opcond

Description

This Tcl command sets the voltage in the operating conditions.

smartpower_set_voltage_opcond -voltage {value} -use {value}

Arguments

ParameterTypeDescription
voltagestringSpecifies the voltage supply in the operating conditions. The acceptable values for this argument are the following:
  • VDD - Sets the voltage operating conditions for VDD.
  • VDD18 - Sets the voltage operating conditions for VDD18.
  • VDDAUX - Sets the voltage operating conditions for VDDAUX.
  • VDDI 1.1 - Sets the voltage operating conditions for VDD 1.1.
  • VDDI 1.2 - Sets the voltage operating conditions for VDDI 1.2.
  • VDDI 1.35 - Sets the voltage operating conditions for VDDI 1.35.
  • VDDI 1.5 - Sets the voltage operating conditions for VDDI 1.5.
  • VDDI 1.8 - Sets the voltage operating conditions for VDDI 1.8.
  • VDDI 2.5 - Sets the voltage operating conditions for VDDI 2.5.
  • VDDI 3.3 - Sets the voltage operating conditions for VDDI 3.3.
  • VDD25 - Sets the voltage operating conditions for VDD25.
  • VDDA - Sets the voltage operating conditions for VDDA.
  • VDDA25 - Sets the voltage operating conditions for VDDA25.
  • VPP - Sets the voltage operating conditions for VPP.
usestringSpecifies the voltage in the operating conditions for each voltage supply. The acceptable values for this argument are the following:
  • oprange - Sets the voltage in the operating conditions as specified in your Project Settings.
  • design - Sets the voltage in the operating conditions as specified in the SmartPower design-wideoperating range. Applies to SmartPower only.
  • mode - Sets the voltage in the operating conditions as specified in the SmartPower mode-specificoperating range. Applies to SmartPower only.
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
Parameter 'use' has illegal value.
Required parameter 'use' is missing.
Parameter 'voltage' has illegal value.
Required parameter 'voltage' is missing.
Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_set_voltage_opcond -voltage "VDD | VDD18 | VDDI 1.8 | VDD25" -use "oprange | design | mode"'.

Supported Families

PolarFire®
SmartFusion® 2
RTG4™
IGLOO® 2
PolarFire SoC

Example

This example sets the VCCA as specified in the SmartPower mode-specific settings:

smartpower_set_voltage_opcond -voltage {VDD} -use {mode}

See Also