21.9.30 smartpower_remove_pin_frequency

Description

This Tcl command removes the frequency associated with a specific pin. This pin will have a default frequency based on its domain.

Note: The pin_name must be the name of a pin that already exists in the design and already belongs to a domain. Execute the "smartpower_commit" Tcl command for preserving any changes in SmartPower.
smartpower_remove_pin_frequency -pin_name {pin_name}

Arguments

ParameterTypeDescription
pin_namestringSpecifies the name of the pin for which the frequency will be removed.
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
NoneRequired parameter 'pin_name' is missing.
NoneParameter 'pin_name' is missing or has invalid value.
NoneParameter 'param_name' is not defined. Valid command formatting is 'smartpower_remove_pin_frequency [-pin_name "name of pin"]+'.

Supported Families

PolarFire®
SmartFusion® 2
RTG4™
IGLOO® 2
PolarFire SoC

Example

The following example removes the frequency from the pin named "d_in":

smartpower_remove_pin_frequency -pin_name {d_in}

See Also