vcd_file | string | Specifies the path to the *.vcd file that you want to import. |
style | string | Specifies the format in which the report will be exported. The acceptable values for this argument are the following: - Text - The report will be exported as Text file.
- CSV(by default) - The report will be exported as CSV file.
|
partial_parse | boolean | Specifies whether to partially parse the *.vcd file. The acceptable values for this argument are the following: - TRUE, true or 1 - Partially parses the *.vcd file.
- FALSE, false or 0 - Does not partially parse the *.vcd file.
|
start_time | decimal | This option is available only if -partially_parse is set to true. Specifies the start time (in ns) to partially parse the *.vcd file. |
end_time | decimal | This option is available only if -partially_parse is set to true. Specifies the start time (in ns) to partially parse the *.vcd file. |
auto_detect_top_level_name | boolean | Specifies whether to automatically detect the top-level name. The acceptable values for this argument are the following: - TRUE, true or 1 - Automatically detects the top-level name.
- FALSE, false or 0 - Does not automatically detect the top-level name.
|
top_level_name | string | Specifies the top-level name. |
report_type | string | Specifies the report query type. The acceptable values for this argument are the following: - activity - Includes activity information for each net.
- power - Includes power information for each net.
- activity and power - Includes activity and power information for each net.
|
report_query | string | Specifies the report type. The acceptable values for this argument are the following: - Report by Net - summary - Provides a summary report for each net.
- Report by Net - detailed - Provides a detailed report for each net.
- Report by Cycle - summary - Provides a summary report for each cycle.
- Report by Cycle - detailed - Provides a detailed report for each cycle.
|
sortby | string | Specifies how to sort the values in the report. The acceptable values for this argument are the following: - total power - Sorts based on the power values.
- spurious power - Sorts based on the spurious power.
- functional power - Sorts based on the functional values.
- spurious transitions - Sorts based on the spurious transitions.
- functional transitions - Sorts based on the functional transitions.
|
sortorder | string | Specifies the sort order of the values in the report. This could be descending or ascending. |
max_net | integer | Specifies the maximum number of nets to report. In a net summary or net details report, this argument limits the total number of entries. In a cycle details report, this argument limits the number of nets reported for each cycle. |
max_cycle | integer | Specifies the maximum number of cycles to report. In a cycle summary or cycle details report, this argument limits the total number of entries. In a net details report, this argument limits the number of cycles reported for each net. |
clock_settings | string | Specifies the settings for the clock. The format is ">clock name<:>active edge {value}<". The acceptable values for this argument are the following: - rising - Sets the clock to a rising active edge.
- falling - Sets the clock to a falling active edge.
- both - Sets the clock to both rising and falling active edge.
- not_active - Does not use the signal as a clock.
|
glitch_filtering | string | Specifies whether to use glitch filtering. The acceptable values for this argument are the following: - TRUE, true or 1 - Glitch filtering is on.
- FALSE, false or 0 - Enables automatic glitch filtering. This option will ignore any value specified in -glitch_threshold.
- auto - Glitch filtering is off.
|
glitch_threshold | integer | This option is only available when -glitch_filtering is set to true. Specifies the glitch filtering value(in ps). |
auto_construct_clock_domain | boolean | Specifies whether to automatically construct the clock domain. The acceptable values for this argument are the following: - TRUE, true or 1 - Automatically constructs the clock domain.
- FALSE, false or 0 - Does not automatically construct the clock domain.
|
clock_period | decimal | Use this option to specify a virtual clock period (in ps). This should be used if -auto_construct_clock_domain is set to false. |
clock_offset | decimal | Use this option to specify the time of the first active edge of the virtual clock (in ps). This should be used if -auto_construct_clock_domain is set to false. |
opmode | string | Use this option to specify the mode from which the operating conditions are extracted to generate the report. - Active - The operating mode is set to Active.
- Flash*Freeze - The operating mode is set to Flash*Freeze.
|
filename | string | Specifies the name or path of the file to be exported. This argument is mandatory. Default created under designer/<root_name> dircetory. |