21.9.19 smartpower_init_set_clocks_options
(Ask a Question)Description
This Tcl command initializes the clock frequency options of all clock domains.
Note: This command is associated with the functionality of Initialize frequencies and probabilities dialog box.
smartpower_init_set_clocks_options [-with_clock_constraints {value}] \
[-with_default_values {value}] \
[-freq {value}] \
[-duty_cycle {value}]
Arguments
Parameter | Type | Description |
---|---|---|
with_clock_constraints | boolean | This sets the option of initializing the clock frequencies with frequency constraints from SmartTime. The acceptable values for this argument are the following:
|
with_default_values | boolean | This sets the option of initializing the clock frequencies with a user input default value. The acceptable values for this argument are the following:
|
freq | string | Specifies the user input frequency in Hz, KHz or MHz. |
duty_cycle | decimal | Specifies the user input duty cycles in percentage(%). |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'duty_cycle' has illegal value. |
None | Parameter 'duty_cycle' must be less than or equal to 100.000. |
None | Parameter 'duty_cycle' must be a positive decimal value. |
None | duty_cycle: Invalid argument value: 'value' (expecting decimal value). |
None | Parameter 'freq' has illegal value. |
None | freq: Parameter format incorrect (expecting a positive decimal value, optionally followed by a unit (possible values are Hz, KHz or MHz)). |
None | Parameter 'with_default_values' has illegal value. |
None | with_default_values: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0 or false). |
None | Parameter 'with_clock_constraints' has illegal value. |
None | with_clock_constraints: Invalid argument value: 'value' (expecting TRUE, 1, true, FALSE, 0 or false). |
None | Parameter 'param_name' is not defined. Valid command formatting is 'smartpower_init_set_clocks_options [-with_clock_constraints "TRUE | FALSE"] [-with_default_values "TRUE | FALSE"] [-freq "decimal value [ unit { Hz | KHz | MHz } ]"] [-duty_cycle "decimal value"]'. |
Supported Families
PolarFire® |
SmartFusion® 2 |
RTG4™ |
IGLOO® 2 |
PolarFire SoC |
Example
The following example initializes all clocks after executing "smartpower_init_do":
smartpower_init_do with -clocks {true}
smartpower_init_set_clocks_options -with_clock_constraints {true} \
-with_default_values {true} \
-freq {10 MHz} \
-duty_cycle {20}