TCPIP_DNS_Enable Function
C
bool TCPIP_DNS_Enable(
TCPIP_NET_HANDLE hNet,
TCPIP_DNS_ENABLE_FLAGS flags
);
Description
This function enables the DNS Client name resolution for the specified interface. The additional flags give better control on how the name resolution is performed.
Preconditions
The DNS module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| hNet | Interface to enable the DNS Client on. |
| flags | Specify further attributes for this interface: act as a strict, preferred or default interface. |
Returns
True - If successful.
False - If unsuccessful: the requested interface could not be selected for DNS name resolving.
Remarks
The interface selection for the name resolution tries to find a valid interface, i.e. an interface that is up and has a valid DNS server. The selection is done following these rules:
if a strict interface is set, only that interface is used for name resolution
else if there is a preferred interface, that one will be tried first
else the default interface is used
else any available interface will be used
Additionally, if a retry is attempted using the same selected interface, an alternate DNS server from that interface will be selected, if available.
Only one strict interface can exist at any time. Selecting a new strict interface will replace the old one.
Only one preferred interface can exist at any time. Selecting a new preferred interface will replace the old one.
The selected interface has to be up and running for the call to succeed.