TCPIP_DNS_IsResolved Function
C
TCPIP_DNS_RESULT TCPIP_DNS_IsResolved(
const char* hostName,
IP_MULTI_ADDRESS* hostIP,
IP_ADDRESS_TYPE type
);
Description
Call this function to determine if the DNS resolution of an address has been completed. If so, the resolved address will be provided in hostIP.
Preconditions
TCPIP_DNS_Resolve() has been called.
Parameters
| Parameters | Description |
|---|---|
| hostName | A pointer to the null terminated string specifying the host for which to resolve an IP. |
| hostIP | A pointer to an IP_MULTI_ADDRESS structure in which to store the resolved IPv4/IPv6 address if resolution is complete. Could be NULL if not needed. |
| type | type of address needed: IP_ADDRESS_TYPE_IPV4/IP_ADDRESS_TYPE_IPV6/IP_ADDRESS_TYPE_ANY. |
Remarks
The function will set either an IPv6 or an IPv4 address to the hostIP address, depending on what's available.
If type IP_ADDRESS_TYPE_ANY is specified the hostIP will be updated with the first available solved address: either IPv6 or IPv4.