TCPIP_DNS_GetIPv4Addresses Function
C
int TCPIP_DNS_GetIPv4Addresses(
const char* hostName,
int startIndex,
IPV4_ADDR* pIPv4Addr,
int nIPv4Addresses
);
Description
This function will return IPv4 addresses for a host name if the DNS resolution has been completed.
Preconditions
TCPIP_DNS_Resolve() has been called.
Parameters
| Parameters | Description |
|---|---|
| hostName | A pointer to the null terminated string specifying the host name. |
| startIndex | Starting index of the IP address to be returned when multiple addresses are available. The max number of addresses that can be stored for a host name is given by TCPIP_DNS_CLIENT_MODULE_CONFIG::n4Entries. The current number of valid entries for an address is given by TCPIP_DNS_GetIPAddressesNumber(). A valid index is [0, TCPIP_DNS_GetIPAddressesNumber(IP_ADDRESS_TYPE_4)). |
| pIPv4Addr | Pointer to array of IPv4 addresses to store the host 4 addresses. |
| nIPv4Addresses | Number of IPv46 addresses in the p4Addr array. |
Returns
> 0 - The number of addresses copied to the p4Addr array.
0 - If the host name was not found, invalid index, bad parameter, etc.
Remarks
None.