TCPIP_DNS_CLIENT_CACHE_ENTRY_TMO Macro
C
#define TCPIP_DNS_CLIENT_CACHE_ENTRY_TMO 0
Description
DNS client cache entry time-out. If this symbol is zero then the entry time-out will be the one specified by the DNS server when the name was solved. Otherwise this value will be used as the cache entry time-out. Default should be 0.