TCPIP_DNS_Resolve Function
C
TCPIP_DNS_RESULT TCPIP_DNS_Resolve(
const char* hostName,
TCPIP_DNS_RESOLVE_TYPE type
);
Description
This function attempts to resolve a host name to an IP address. When called, it will attempt to send a DNS query to a DNS server for resolving the name. Call TCPIP_DNS_IsResolved to determine if name resolution is complete.
Preconditions
DNS client module initialized.
Parameters
| Parameters | Description |
|---|---|
| hostName | A pointer to the null terminated string specifying the host for which to resolve an IP. |
| type | A TCPIP_DNS_RESOLVE_TYPE value specifying the desired resolution. |
Returns
TCPIP_DNS_RES_OK - Success, name is solved.
TCPIP_DNS_RES_PENDING - Operation is ongoing.
TCPIP_DNS_RES_NAME_IS_IPADDRESS - Name request is a IPv4 or IPv6 address.
An error code if an error occurred.
Remarks
To clear the cache use TCPIP_DNS_Disable(hNet, true);