TCPIP_DNS_Send_Query Function
C
TCPIP_DNS_RESULT TCPIP_DNS_Send_Query(
const char* hostName,
TCPIP_DNS_RESOLVE_TYPE type
);
Description
This function attempts to send a query packet for the supplied host name and DNS type.
Preconditions
The DNS client module must be initialized.
Parameters
| Parameters | Description |
|---|---|
| hostName | A pointer to the null terminated string specifying the host for which to resolve an IP. |
| type | A TCPIP_DNS_RESOLVE_TYPE value specifying the desired resolution. |
Returns
TCPIP_DNS_RES_OK - Success, name is solved.
TCPIP_DNS_RES_PENDING - Operation is ongoing.
TCPIP_DNS_RES_NAME_IS_IPADDRESS - Name request is a IPv4 or IPv6 address.
An error code if an error occurred.
Remarks
If the name is already part of the DNS resolution process (has been previously requested with TCPIP_DNS_Resolve or TCPIP_DNS_Send_Query) the function will force a new DNS query . If the name resolution is already solved and completed, this function will mark it as incomplete and a new response from the server will be requested.
If the name was not part of the DNS client resolution, then this function is equivalent to TCPIP_DNS_Resolve().