| General Functions | |
| TCPIP_DNS_HandlerDeRegister | Deregisters a previously registered DNS client handler. |
| TCPIP_DNS_HandlerRegister | Registers a DNS client Handler. |
| TCPIP_DNS_IsEnabled | Determines if the DNS client is enabled on that specified interface. |
| TCPIP_DNS_ClientInfoGet | Get the current DNS client parameters. |
| TCPIP_DNS_ClientTask | Standard TCP/IP stack module task function. |
| TCPIP_DNS_Disable | Disables the DNS Client for the specified interface. |
| TCPIP_DNS_Enable | Enables the DNS Client for the specified interface. |
| TCPIP_DNS_EntryQuery | Queries a DNS Resolver specific entry. |
| TCPIP_DNS_GetIPAddressesNumber | Get the count of resolved IPv4 and/or IPv6 address for a host name. |
| TCPIP_DNS_GetIPv4Addresses | Get IPV4 addresses for a DNS resolved name. |
| TCPIP_DNS_GetIPv6Addresses | Get IPV6 addresses for a DNS resolved name. |
| TCPIP_DNS_IsNameResolved | Determines if the DNS resolution is complete and provides the host IP address. |
| TCPIP_DNS_IsResolved | Determines if the DNS resolution is complete and provides the host IP address. |
| TCPIP_DNS_RemoveAll | Removes all the cached entries from DNS resolver. |
| TCPIP_DNS_RemoveEntry | Remove a hostname from the DNS Hash entry. |
| TCPIP_DNS_Resolve | Begins resolution of an address. |
| TCPIP_DNS_Send_Query | Forces resolution of an address. |
| Data Types and Constants | |
| TCPIP_DNS_EVENT_HANDLER | Notification handler that can be called when a specific entry is resolved and entry is timed out. |
| TCPIP_DNS_EVENT_TYPE | This enumeration is used to notify DNS client applications. |
| TCPIP_DNS_HANDLE | DNS client handle. |
| TCPIP_DNS_RESULT | DNS client result codes. |
| TCPIP_DNS_CLIENT_INFO | General DNS client info. |
| TCPIP_DNS_CLIENT_MODULE_CONFIG | Provides a place holder for DNS client configuration. |
| TCPIP_DNS_ENABLE_FLAGS | Flags for enabling the DNS service on an interface. |
| TCPIP_DNS_ENTRY_QUERY | DNS module query data for both IPv4 and IPv6 . |
| TCPIP_DNS_RESOLVE_TYPE | DNS query record type. |
| TCPIP_DNS_CLIENT_ADDRESS_TYPE | This parameter can be used to choose ithe type of IP connection for the DNS client: IPv4 or IPv6. Currently only IPv4 is supported and this parameter is not used. Reserved for future development |
| TCPIP_DNS_CLIENT_CACHE_DEFAULT_TTL_VAL | Default TTL time for a solved entry in the cache This value will be used when the DNS server TTL value for an entry is 0 |
| TCPIP_DNS_CLIENT_CACHE_ENTRIES | Number of DNS resolver entries |
| TCPIP_DNS_CLIENT_CACHE_ENTRY_TMO | DNS client cache entry time-out. If this symbol is zero then the entry time-out will be the one specified by the DNS server when the name was solved. Otherwise this value will be used as the cache entry time-out. Default should be 0. |
| TCPIP_DNS_CLIENT_CACHE_PER_IPV4_ADDRESS | Maximum and default number of IPv4 answers to be considered while processing DNS response from server for a query. |
| TCPIP_DNS_CLIENT_CACHE_PER_IPV6_ADDRESS | Maximum and default number of IPv6 answers to be considered while processing DNS response from server for a query. |
| TCPIP_DNS_CLIENT_CACHE_UNSOLVED_ENTRY_TMO | Time-out for the a unsolved name, in seconds. The name resolution will be aborted if the TMO elapsed and the name could not be solved Should be greater than TCPIP_DNS_CLIENT_LOOKUP_RETRY_TMO |
| TCPIP_DNS_CLIENT_LOOKUP_RETRY_TMO | Retry lookup for a unsolved entry in the cache, in seconds. If the TCPIP_DNS_CLIENT_LOOKUP_RETRY_TMO seconds elapsed and the name has not been solved then the name entry will be marked with server timeout and the resolution will be retried. Should be less than TCPIP_DNS_CLIENT_CACHE_UNSOLVED_ENTRY_TMO |
| TCPIP_DNS_CLIENT_MAX_HOSTNAME_LEN | Max DNS host name size Use an appropriate value, depending on the names that need to be solved |
| TCPIP_DNS_CLIENT_MAX_SELECT_INTERFACES | Max number of interfaces to take part in the DNS selection algorithm Should be always greater than 1: |
| the | default interface should always be considered for DNS resolution |
| Depending | on how many active interfaces select those to be considered for DNS resolution |
| TCPIP_DNS_CLIENT_SERVER_TMO | When the DNS Client connected to the DNS Server this is the elapsed time after which an the communication is considered to have timed failed if there was no reply from the server In seconds |
| TCPIP_DNS_CLIENT_TASK_PROCESS_RATE | DNS Client task processing rate, in milliseconds. The DNS Client module will process a timer event with this rate for processing its own state machine, etc. The default value is 200 milliseconds. The lower the rate (higher the frequency) the higher the module priority and higher module performance can be obtained The value cannot be lower than the TCPIP_STACK_TICK_RATE. |
| TCPIP_DNS_CLIENT_USER_NOTIFICATION | allow DNS client user notification if enabled, the TCPIP_DNS_HandlerRegister/TCPIP_DNS_HandlerDeRegister functions exist and can be used |