17.4.8 Result
When each record is processed by the math sequencer, the math sequencer result can be
stored as defined by Write mode bits WM[1:0] in the ITCLSxCON register. Also, ITCLSxCON
WM[1:0] bits can be overwritten/replaced with other ITCSMATHCMDx WM[1:0] settings in the
math sequencer command. These bits in the math command overwrite the list register
settings WM[1:0] only when the WMOV bit = 1 in the math command. The
following write result options are available:
- WM[1:0] =
0means “always write.” - WM[1:0] =
1means that the math result is stored only when a comparator event is detected. - WM[1:0] =
2means “never write.”
For each record, each math sequencer command stores the result in the corresponding
ITCRESx register as defined by the WM[1:0] bits. The data processed by the math
sequencer can be in unsigned or signed formats. The format is selected by the SIGN bit
in the ITCCON1 register. SIGN bit = 0 means unsigned, and SIGN bit =
1 means signed format. The CVD algorithm accumulates the difference
between Sample A and B. In the case of CVD, the SIGN bit must always be set.
All data in the math sequencer are 24-bit in size. Bit 23 is a sign bit. When the math sequencer's signed result is stored into the 32-bit ITCRESx register, the sign bit is extended automatically.