4.3.12.4 Round Logic
The round logic can perform a conventional (biased) or convergent (unbiased) round function during an accumulator write (store). The Round mode is determined by the state of the Rounding Mode Select (RND) bit (CORCON[1]). It generates a 16-bit 1.15 or 32-bit 1.31 data value, which is passed to the data space write saturation logic. If rounding is not indicated by the instruction, a truncated 1.15 or 1.31 data value is stored.
The two Rounding modes are shown in Figure 4-12. Conventional rounding takes bit 31 of the accumulator, zero-extends it and adds it to the most significant word (msw), excluding the guard or overflow bits (bits 32 through 63). If the least significant word (lsw) of the accumulator is between 0x80000000 and 0xFFFFFFFF (0x80000000 included), the msw is incremented. If the lsw of the accu- mulator is between 0x0000 and 0x7FFFFFFF, the msw remains unchanged. A consequence of this algorithm is that over a succession of random rounding operations, the value tends to be biased slightly positive.
Convergent (or unbiased) rounding operates in the same manner as conventional rounding except when the lsw equals 0x80000000. If this is the case, the LSb of the msw (bit 32 of the accumulator) is examined. If it is ‘1’, the msw is incremented. If it is ‘0’, the msw is not modified. Assuming that bit 16 is effectively random in nature, this scheme removes any rounding bias that may accumulate.
The SAC and SACR instructions store either a truncated (SAC) or rounded (SACR) version of the contents of the target accumulator to data memory via the X-bus (subject to data saturation).
For the MAC class of instructions, the accumulator write-back data path is always subject to rounding. An overflow that occurs as a consequence of a rounding operation will also be subject to saturation.