3.3.8 mcFoc_ClarkeTransformation

C


/* Clarke Transformation */
void mcFoc_ClarkeTransformation( const tmcTypes_ABC_s * pABC, tmcTypes_AlphaBeta_s * const pAlphaBeta )	

Summary

Clarke Transformation

Description

This function performs the Clarke transformation to convert three-phase currents into two-phase alpha-beta currents.

The Clarke transform is a linear transformation, shown in following equation, which can apply to any vector quantity X, although typical examples are voltage V, current I, or flux linkage ψ.

Xα=23XA−13XB−13XC=XA
Xβ=13XA+23XB

The function assumes that the sum of the three-phase values is zero (XA+XB+XC=0), which is a common assumption in balanced three-phase systems.

Precondition

None..

Parameters

ParamDescription
pABC A pointer to the structure holding three-phase currents.
pAlphaBetaA pointer to the structure holding alpha-beta currents.

Returns

None

Example

tmcTypes_ABC_s phaseValues = { .a = 1.0f, .b = 0.5f, .c = -1.5f };
tmcTypes_AlphaBeta_s AlphaBeta;;
mcFoc_ClarkeTransformation(&phaseValues, &AlphaBeta);
    

Remarks

None.