6.2.1 Design Flow
The following steps are used to configure the AHB bus matrix in the application:
- Configure the AHB bus matrix by using the MSS configurator in the application, as shown
in the following figure.
Figure 6-18. AHB Bus Matrix in Libero® SoC Design MSS Configurator - Click AHB Bus
Matrix to configure it. The AHB Bus Matrix configuration window is shown
in the following figure.
- The AHB bus matrix provides support to remap eNVM, eSRAM, and
DDR memory regions to location 0x000000000 of the Cortex-M3 ID code space. It also
provides an option to remap eNVM for a Soft Processor eNVM Remap. To enable
remapping for eNVM, eSRAM, and DDR select appropriate option from remapping
section of AHB Bus Matrix configurator.
Figure 6-19. AHB Bus Matrix Configuration Window - Enter the weight values for the masters in arbitration section, to configure the programmable weight registers MASTER_WEIGHT0_CR and MASTER_WEIGHT1_CR. These are located in the SYSREG block with the required weight values. The weight values range is from 1 to 32.
- Enter the maximum latency values for the fixed priority masters
to configure ESRAM_MAX_LAT registers that are located in the SYSREG block.
This
decides the peak wait time for a fixed priority master arbitrating for eSRAM
access while the WRR master is accessing the slave. Slave maximum latency can be
configured from 1 to 8 clock cycles (8 by default).Important: ESRAM_MAX_LAT is only supported for fixed priority masters addressing eSRAM slaves. It has no effect on WRR masters.
- The AHB bus matrix provides support to remap eNVM, eSRAM, and
DDR memory regions to location 0x000000000 of the Cortex-M3 ID code space. It also
provides an option to remap eNVM for a Soft Processor eNVM Remap. To enable
remapping for eNVM, eSRAM, and DDR select appropriate option from remapping
section of AHB Bus Matrix configurator.
- Generate the component by clicking
Generate Component or by selecting .
For more information on generation of the component, see the latest SmartDesign User Guide on Libero SoC User Guide page.
- Click Generate
Bitstream under Program Design to complete
*.fdbfile generation.Important: The MSS AHB Bus Matrix supports full behavioral simulation models. For more information, see SmartFusion2 MSS BFM Simulation User Guide.