23 Fabric Interface Controller
The fabric interface controller (FIC) enables connectivity between the fabric and the Microcontroller Subsystem (MSS). The FIC is a part of the MSS and performs a bridging function for AHB-Lite to APB or AHB-Lite to AHB-Lite between the AHB bus matrix and the FPGA fabric. The interface type is configurable. There are up to two, 32-bit FICs in SmartFusion 2 devices, referred to as FIC_0 and FIC_1. Both FICs provide two bus interfaces between the MSS and the fabric. The first is mastered by the MSS and has slaves in the fabric; the second is mastered by the fabric and has slaves in the MSS.
The interfaces to the fabric can be 32-bit AHB-Lite or 32-bit APB. The address and data buses between the FIC and the FPGA fabric are overlaid; hence, only one type of interface can be enabled at any time. However, separate groups of signals are used for the AHB-Lite and APB control signals. In addition to the choice of AHBLite or APB interfaces between the MSS and the fabric, a number of options related to relative clock frequencies and pipelining of transactions are available. Each FIC block can operate on a different clock frequency, defined as a ratio of the MSS main clock, M3_CLK.
The SmartFusion 2 architecture imposes a certain number of rules related to clocking domains between the fabric interfaces and the FPGA fabric. This document provides guidance on how to properly construct such systems. The following figure depicts the connectivity of FIC_0 and FIC_1 to the AHB bus matrix.
AHB-Lite master interface and AHB-Lite slave interface of FIC_0 are directly connected with mirrored master 4 (MM4) and mirrored slave 4 (MS4) on the AHB bus matrix. To reduce the load on the AHB bus matrix, FIC_1 AHB-Lite slave interface is connected through the synchronous AHB-to-AHB bridge with an address decoder which inserts a one-cycle delay in each direction.
The following table lists the number of FICs available for use in each device.
| Device | FIC Blocks |
|---|---|
| M2S005 | 11 |
| M2S010 | |
| M2S025 | |
| M2S050 | 2 |
| M2S060 | 1* |
| M2S090 | |
| M2S150 | 2 |
- Only FIC_0 is available.