21.6.2.15.2 Function system_gclk_chan_set_config()
Writes a Generic Clock configuration to the hardware module.
void system_gclk_chan_set_config( const uint8_t channel, struct system_gclk_chan_config *const config)
Writes out a given configuration of a Generic Clock configuration to the hardware module. If the clock is currently running, it will be stopped.
Note: Once called the clock will not be running; to start the clock, call system_gclk_chan_enable() after configuring a clock channel.
| Data direction | Parameter name | Description |
|---|---|---|
[in] | channel |
Generic Clock channel to configure |
[in] | config |
Configuration settings for the clock |