29.4.6.3 Wait for Software Trigger
The user can set either a ‘PTGCTRL 0b1011’ (edge-triggered) or
‘PTGCTRL 0b1010’ (level-triggered) command to wait for a software
generated trigger. This trigger is generated by setting the PTGSWT bit (PTGCON[10]).
The ‘PTGCTRL 0b1011’ command is sensitive only to the PTGSWT bit
transition from ‘0’ to ‘1’. This transition must occur
during the command execution; otherwise, the command will continue to wait. The PTGSWT
bit is automatically cleared by hardware on completion of the ‘PTGCTRL
0b1011’ command execution, initializing the bit for the next software
trigger command.
Figure 29-7 explains the operation of the wait for an edge-based software trigger.
The ‘PTGCTRL 0b1010’ command is sensitive to the level of the PTGSWT
bit. This command waits until PTGSWT = 1. It will complete immediately
if PTGSWT = 1 upon entry to the command. The PTGSWT bit is not
automatically cleared by the ‘PTGCTRL 0b1010’ command. If desired, the
PTGSWT bit can be cleared by the user application on completion of the ‘PTGCTRL
0b1010’ command execution. Figure 29-8
explains the operation of the wait for the level-based software trigger.
Using the ‘PTGCTRL 0b1010’ or ‘PTGCTRL 0b1011’ step
commands halts execution of further commands until the PTGSWT bit is set, allowing the
user to coordinate activity between the PTG module and the application software.