2.39.3 EFC_QuadWordWrite Function
C
bool EFC_QuadWordWrite( uint32_t* data, uint32_t address )
Summary
Writes a 128-bit data to a given address in FLASH memory.
Description
This function takes a 32-bit address, a pointer to the 128-bit data and writes it to the given location in FLASH memory.
Precondition
Validate if EFC controller is ready to accept new request by calling EFC_IsBusy() The Memory to be written should be in Erased State.
Parameters
Param | Description |
---|---|
address | FLASH address to be modified |
data | pointer to 128-bit data buffer |
Returns
Always returns true.
Example
uint32_t data[4]; data[0] = 0x12345678; data[1] = 0x87654321; data[2] = 0x12345678; data[3] = 0x87654321; EFC_QuadWordWrite((uint32_t *) data, 0x500000); while(EFC_IsBusy());
Remarks
Application needs to poll for busy bit or wait for callback to be called before sending next request.