2.39.12 EFC_PageBufferCommit Function
C
bool EFC_PageBufferCommit( const uint32_t address)
Summary
Commits the data present in EFC internal latch buffer to flash memory
Description
Writes data loaded in the EFC internal latch buffer to the flash memory.
Precondition
The EFC_Initialize() function should have been called once.
Parameters
Param | Description |
---|---|
address | Data Flash address to be modified. |
Returns
true if the operation was successful, else returns false.
Example
uint32_t* data; //data - pointer to the buffer to be written to flash memory
uint32_t flashAddr; //flashAddr - variable containing flash address
//populate data and flashAddr
EFC_PageBufferWrite((uint32_t*)data, (uint32_t)flashAddr);
//update data here
EFC_PageBufferWrite((uint32_t*)data, (uint32_t)flashAddr);
//Commit the final data in the EFC internal latch buffer to the flash memory
EFC_PageBufferCommit((uint32_t)flashAddr);
//Wait until the EFC controller is busy
while (EFC_IsBusy());
Remarks
None