2.39.5 EFC_SectorErase Function
C
bool EFC_SectorErase( uint32_t address)
Summary
Erases a Sector in the FLASH.
Description
This function is used to erase a sector (collection of pages).
Precondition
Validate if EFC controller is ready to accept new request by calling EFC_IsBusy()
Parameters
Param | Description |
---|---|
address | FLASH address to be Erased |
Returns
Always returns true.
Example
EFC_SectorErase(0x500000);
while(EFC_IsBusy());
Remarks
Application needs to poll for busy bit or wait for callback to be called before sending next request.