2.90.5 RNG_Seed1Get Function
C
uint32_t RNG_Seed1Get (void);
Summary
Returns the content of RNGSEED1 register.
Description
This function is used to read the Least Significant Byte 32-bits of the TRNG number (from RNGSEED1 register).
Precondition
None.
Parameters
None.
Returns
Contents of RNGSEED1.
Example
uint32_t seed1 = 0;
seed1 = RNG_Seed1Get();
Remarks
Use together with RNG_Seed2Get() if the required bits length is more than 32-bits.