2.90.17 RNG_NumGen1Get Function

C

uint32_t RNG_NumGen1Get (void);

Summary

Returns the value in the RNGNUMGEN1 register.

Description

When the PRNG operation is finished, RNGNUMGEN1 register contains the LSB 32-bits of the current random number in the PRNG. This function can be used to read the generated random number.

Precondition

None.

Parameters

None.

Returns

The LSB (32-bits) of the pseudo-random number generated in PRNG.

Example

uint32_t numgen1 = 0;
numgen1 = RNG_NumGen1Get();

Remarks

None.